Hello to everybody,
i have a question on "Rerouting The Right Leg Drive Signal".
I have closed the loop as seen in figure 51 in the datasheet. Then i connected the RLD Electrode to the IN2P Pin.
Now i think i only have to set the MUX2[2:0] = 110 in the CH2SET Register and set the RLD2P Bit in the RLD_SENSP Register to zero.
Is that right or are there more necessary settings?
Regards,
Sebastian