This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS8556 parameter values calculation

Other Parts Discussed in Thread: ADS8556

Hi,

 

On page 35 of the datasheet (http://www.ti.com/lit/ds/symlink/ads8556.pdf) there are suggested values for Rf and Cf for the highest data rate. If the ADC is to be run at 150kSPS maximum, what would the suggested values be for those parameters? Thanks in advance.

 

Regards,

 

Brian Wang

  • Hi Brian,

    Which range do you plan on using with the ADS8556?  Running the device at 150Ksps would give you over 5us sampling time, so in the 4x mode, you could go as high as 1200 ohms and 390pF.  In 2x mode, something like 560ohms and 820pF would be a good starting point.