Other Parts Discussed in Thread: ADS8320
Hi there,
Im getting stucked lately using an ads8320 connected to my microcontroller, an Atmega1281. The problem is that I have no signal in the DOUT pin of the converter and I cant figure why.
This is the image from the oscilloscope:
I have checked carefully the connections and everything seems right.
My code is the following:
//Variables globales
unsigned char data=0x01,data1=0x3D,aux2,adc1,adc2,adc3,todouno=0xFF;
//int adc=0x00;
//Mis funciones
void SPI_MasterInit(void);
void writetoreg(unsigned char);
unsigned char readdata(unsigned char data);
void resetADC(unsigned char cDataH);
void _delay_ms (double __ms);
unsigned char readfromreg(unsigned char data8);
int main(void)
{
//Configurar puertos e inicializar
SPI_MasterInit();
sei();
while(1)
{
//read 16 bits data
PORTB = (0<<PB0)|(1<<PB4)|(1<<PB5);//cs low
adc1=readdata(todouno);
adc2=readdata(todouno);
adc3=readdata(todouno);
PORTB = (1<<PB0)|(1<<PB4)|(1<<PB5);//cs high
}
}
void SPI_MasterInit(void)
{
/* Set MOSI,SS and SCK output, all others input */
DDRB = (1<<DDB1)|(1<<DDB2)|(1<<DDB0)|(1<<DDB4)|(1<<DDB5);
PORTB = (1<<PB0)|(1<<PB4)|(1<<PB2);//fsync disp1
/* Enable SPI, Master, set clock rate fck/16 , MSB first*/
SPCR = (1<<SPE)|(1<<MSTR)|(1<<SPR0)|(0<<DORD)|(1<<CPOL)|(0<<CPHA);
}
unsigned char readdata(unsigned char data)
{
//PORTB = (0<<PB0)|(1<<PB4)|(1<<PB5);//cs low
unsigned char adc;
SPDR = data;
adc = SPSR;
// Start transmission
while(!(SPSR & (1<<SPIF)));
adc = SPSR;
//PORTB = (1<<PB0)|(1<<PB4)|(1<<PB5);// cs high
return adc;
}
Any help or tip you could give would help me a lot. Thanks
Regards, Daniel.