Hello,
I have two analog inputs, one from a light level sensor ranging from 3mV to 3V, and the other a conditioned and amplified signal from an RTD ranging from ~1.5 to 3V. I will only need to monitor these sensors every second or so, so speed is not an issue. Vcc=+3.3V
I am trying to determine if a sigma-delta or SAR ADC is more suited to this application. From my reading it seems that either would be fine, except for one point I read here (http://www.cypress.com/?rID=43323). This article states that sigma-delta converters have non-linearity at the end-points of the scale and should not be used in applications that require linearity rail-to-rail. Would this be a problem with the ADS1015, and specifically would it affect my application?
Thanks in advance,
Aaron