hi,
i've experienced some offset problems when using the ads 1232 with a 0.5mv/V load Cell. Because of the low sensitivity of the load cell i'm using a reduced Vref of 1.666V (5V/3 ) in a ratio metric configuration (voltage divider) and a gain of 128. (VREFN 0V, AVDD and DVDD 5V, 0.1uF HQ poly as Bypass cap, clean vref and supply, using a ground plane, no supply loops and caps near ADC)
To figure out where the offset comes from i've shorted AINP and AINN and put it on 2.5V potential to not violate the conmen mode condition. After offset calibration (26 sclk's) the result should be a noise around zero.
Everthing works fine when using 5V Vref . But when using the reduced Vref there is a large offset error. In general the measurements are fine with 1.666 Vref, SNR is 3 times better compared to 5V Vref, linearity is fine. But i really like to understand where this offset error comes from and i can't see violation of the specs.
Are there any reported problems?
Best Regards