This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1298 Register Read/Write

Hello everbody,

writing to the registers now works fine. DRDY toggles at 2ms (500SPS), as i want.

But when i read out the register i always get a value which is shifted one point to the right.

For example: 

value for CONFIG1: 0x86(1000|0110)

return value:             0x43(0100|0011)

value for CONFIG3: 0xDC(1101|1100)

return value:             0x6E(0110|1110)

What can be the reason for this??

regards,

Sebastian