Other Parts Discussed in Thread: THS4521, ADS1278, ADS8321, ADS1178, ADS1174
What's the difference between the two implementations? One configuration appears to shunt HF and noise, but would allow the opamp to oscillate if induced. The other configuration would provide the same LP filter and also reduce potential for opamp oscillation. Am I viewing these correctly?
According to Jim Karki's work, the two shunt capacitors should be 2x of the differential capacitor. Why is the capacitor pictured below a 1nF (from the THS4521 datasheet), whereas it should be 33pF?
The circuit below puts the capacitors in the feeback loop. This would (1) reduce capacitive loading on the opamp's output, and (2) dramatically reduce gain for increasing frequency, thereby reducing parasitic oscillations. Why is this topology far less published as reference circuits in datasheets, etc?