Other Parts Discussed in Thread: ADS8028
I need to check the current taken from an EXTERNAL VREF (5V) on the REF pin once the software has switched to select the external REF.
The datasheet does not seem to state this explicitly (or very clearly anyway).
The data sheet (March 2012 update) page 4 states DC leakage as +/- 0.01uA with +/-1uA as the MAX. This implies the MAX current taken/sourced by this pin will be +/-1uA once the EXT REF has been selected.
However on page 15 under REFERENCE it says the INTERNAL reference can supply up to 2mA 'and is designed to drive the ADS8028' this implies an EXT REF may have to supply up to 2mA unless the ADS8082 actually buffers any EXT REF and that this buffer is supplied from AVDD. I need to know whether to buffer my EXT REF and how much current it must supply.
Many thanks