Dear Kevin,
I am a bit glad i am not the only one who gets confused when reading the REFN REFP part of the datasheet. Since we have already decided to use the 1298 in a new project it would save me time if I understand it before mounting a 1st board version. We are thinking on using a +/- 2.5V suply, couse we need to have the patient at the 0V of the system. The questions are:
1) I must link VREFN to AVSS right?
2) I believed until now (considering the answer for question 1 is yes), I could link 0V to VREFP, but in fact it must be positive is that it?
3) If I use a +/-2.5V supply, gain = 1 and a xV VREFP wich voltages are the full scale to the converter?
Thanks for your attention,
Paulo Farina