Other Parts Discussed in Thread: MSP430F4617, ADS1291
Good Day,
I'm using an ADS1291 AFE along with a MSP430F4617.
After making all the connections according to the datasheet, I am able to connect to the device using SPI and configure the registers, but I am not able to start capturing data, and setting the clock output bit in the CONFIG register would not output the clock in the CLK pin, even when the CLK_SEL pin is set high.
I also tried supplying an external 512Khz clock with CLK_SEL low and it would still not allow me to capture.
is there any setting or connection I could test out before calling it DOA?
I'm sure I'm missing out something as I currently have 2 1291 chips misbehaving the same way
Thanks