Other Parts Discussed in Thread: ADS4149, OPA690
Over the course of my career, I have learned that an op-amp must have an open loop gain greater than the number of bits of the ADC it is driving to prevent the effects of DC gain error (note: no the effects of GBW). For example, a 14 bit converter should have an open loop gain >=2^14, or 16,384 V/V, or 84.3 dB. Similarly, at 16 bits, the open loop gain should be >= 2^16, or 65,536 V/V, or 96.3 dB. What I cannot find is how to determine the effects this has on an ADC perfromance. i.e if I feed a 14 bit ADC with a "12 bit amplifier", what difference does it make to the ADC representation of the system input signal?
I have been looking around the literature for a while (here and other places) and have not found anything that directly addresses the question.