Hi to everyone.
Someone can to help me. I looking for code example to use ADC (ADS7863). It use SPI interface.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi to everyone.
Someone can to help me. I looking for code example to use ADC (ADS7863). It use SPI interface.
Hi Yuri,
Welcome to our forum! Is there any particular processor you have in mind to use with the ADS7863?
Hi Yuri,
I have no SPI examples for the Raspberry Pi, however, there are several code snippets available for the ADS8361 and ADS7861 on various TI processors here: http://www.ti.com/product/ads8361#doctype1
The ADS8361 and ADS7861 are early version of the ADS7863, they did not have the internal reference, so there are no actual 'registers' to configure.
Tom Hendrick said:however, there are several code snippets available for the ADS8361 and ADS7861 on various TI processors here: http://www.ti.com/product/ads8361#doctype1
i can't to find the examples.
Yuri,
Did you have any luck finding some example code? I also want to interface to a ADS7863 although I am using a TI MSP430F5528. I have used the built in SPI port before and I'm sure I can figure it out but some example code would be a big help.
Mike
Hi Yuri,
How are you making out here? I'll see what I can do about getting you some example code after the first of the new year.