I am using and agilent es3631a power supply to provide the 2426 with 6 volts but the current is larger than the 170uA operation or 20mA source current capacity. I don't understand how to set up the 2426 to handle 20 - 30 volts but still be within the current capacity of the device. Any help would be appreciated. Thanks.