Other Parts Discussed in Thread: LMX2531
Hello,
I am using the ADC12D1X00RFRB board with the Wave Vision 5 software and I am have some difficulty changing the default internal clock frequency. I would like to set it to 1830MHz or as close to that as possible. The default clock frequency is 1590MHz and the eval board's manual says that the LMX2531 Clock Synthesis chip is configured for a frequency the range of 1530-1636MHz / 1726-1840MHz through the serial interface which may be controlled through the WaveVision 5 register control panel. Does anyone know which register is used to control this clock chip?
Thanks in advance for your help.
Brian Fisher