Other Parts Discussed in Thread: ADS1252, ADS1274, DDC264EVM, DDC264, ADS1259, ADS1258, ADS1259EVM-PDK, ADCPRO
Hi all,
I am designing a 24 bit system that reads the analog voltage from an integrator every 0.1 to 1 Millisecond. The output of the integrator is essentially a step function. The integrator clears as soon as the ADC is done, before the next integration at 1-10Khz.
The only part I see that can do this with power dissipation lower than 100mw is the ADS1252. I need 256 channels of simultaneous conversion. With 5 Conversion settling time @ 41.7Khz ODR = about 144 microseconds, but the BW is only 9Khz =about 100 usec rise time.
The ADS1274 has a higher bandwidth (48Khz) but a longer settling time (739 usec), so I am limited to 1/739 usec as a rep rate for step functions (1353 Hz).
What is the best ADC to use for this?
Pd = <100mw
Step response to DOUT <100 usec.
18-20 bits effective