Other Parts Discussed in Thread: DAC7562, CD4504B
Hello,
I'm having trouble getting my DAC to do, well, anything. My pin configurations are:
GND to ground
!LDAC to ground
!CLR to 5V
VREF to a capacitor (using internal reference)
AVDD to 5v
DIN, SCLK, and !SYNC to a mess really.
The outputs I have access to put out 12V, so I've had to send the 12V from those into a resistor. Let's call the other side of the resistor node A. Node A connects to a Schottkey diode which leads into 5V. This puts node A at around 5.5V when 12V is applied and 0 when nothing is applied. I use the 5.5V for the DIN, SCLK, and !SYNC lines.
Here are my wave forms.
Blue is my data and red is my clock signal. I realize I'm running extremely slow, but once I figure out my problem, I'm going to speed things up.