Other Parts Discussed in Thread: ADS1259
Hi there,
I'm just reading through the datasheet of the ADS1259 and the given values for the typical and maximal gain error keep confusing me.
According to the electrical characteristics section, the typical (uncalibrated) gain error is 500ppm@25°C and the maximal gain error is 5000ppm@-40 to +105°C. But according to the plots in the typical characteristics section, none of five units even reaches the typical value (which is sort of contrary to the meaning of the word "typical"). The range of the gain errors in the "gain error and offset vs reference voltage" figure is even ten times lower than 500ppm and almost zero at 2.5V Vref. I know that this device can be calibrated, but from my understanding, these plots should not show any calibrated measurements. Why do the values for the gain error differ so much Could somebody please clear those things up? Thanks in advance!