Hi,
I am working on a project where the DAC3i62EVM is connected to the FMC connector on a Spartan6 SP601 Evaluation board. We are generating a gaussian wave for RF pulse shaping in a high power amplifier. I plan to drive the EVM with 200 MHz clock from the FPGA board. My question is if set the output to 1.8V will this work with the CDCP1803 clock chip on the eval board. Will it work with the square wave clock from the FPGA?
thanks
Stan Vaughn