I am planning to use the ADS1298 to measure 7 thermistors (10K) each with. I create a voltage divider with a 112k resistor therefore the max current for each sensor is 10uA. Can I connect these sensors to the output of the voltage reference in order to have a ratiometric reading. The max current I will be taking is going to be 100uA.