I am designing a control system based on the DAC8728 and TMS320F28335, and they are connected directly by the buses(including data bus, address bus and control bus). The schematic is shown as below.
The analog output VOUT-1(pin10) is set by writing to the space with the address of 0x0020023E in ZONE7, and followed by write the configuration register with the address of 0x0020003E to set the LD bit. However, the analog output is always 0V, no matter how I change the input digital data. I have checked the PCB solding, DSP output, and others I can think of, and all of them are OK.
Could you give me some suggestings? Thank you!