This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

need some help on THS1206EVM

Other Parts Discussed in Thread: THS1206

Hi  TeVERYONE

Could you help me in this  THS1206 evm- :

Iam providing an analog input of 0.1 -0.2v to AINP and GND to obtain its digital form using THS1206EVM . .But i am not able to obtain the outputs. I also have few doubts which are described below-

Is the pin Avdd,Dvdd,Bvdd ,to be connected to power supply?What is the ideal supply votage to be given ?

Where should i apply the reference voltage , i.e, at +ref & -ref or at refp & refm ?

What about the connections to the pin - 5VA ,5VD,3.3V,REFIN ? are those pins to be left open ?

And in the j1 the unused odd pins are to be grounded externally or are they grounded internally?

If possible could you mark the pins in this image ?