Other Parts Discussed in Thread: ADS8363, AFE0064
Hi,
I'm trying to use the ADS8363 to convert the output of two AFE0064. The ADS is set to work in fully-differential, simoultaneous, half-clock mode. I set both references REFIO1 and REFIO2 to 1.4V. Now, I wanted to change the reference thinking that REFIO1 wuold effect CH0A/B and REFIO2 for CH1A/B, instead I noticed that only REFIO1 has effect on the output and it does for all the four channels, is that correct?
I am using two external references for REFIO1 and 2, and I did not change anything on the register, as everything else is as default, any hint for that?
thanks a lot
Iolanda