Hi,
I have a little problem with driving ADC (ADS1672) from high impedance source of low-frequency differential signal.
This ADC clocking by 10 MHz oscillator and according Fig.22 of datasheet (SBAS402D) effective input impedance is 6.25 kOhm. Fig.40 shows a "Basic Differential Input Signal Interface" with 600 Ohm input impedance presumably. Can I increase input impedance of the Basic Circuit by replacing 392 Ohm resistor to 100 kOhm? Whether there are more preferred schematic approaches, OpAmps, etc.?
PS: The signal source must be DC-coupled with ADC and frequency range is DC-10 kHz. Sampling rate is about 39kSPS.
PPS: Sry for silly question :)