Other Parts Discussed in Thread: ADS1248
Hi,
I'm using an ADS1248EVM board for a pH sensor, my settings are AVDD +2.5 AVSS -2.5 PGA 1, using internal reference, single ended with the AIN0 to pH sensor and AN1-AIN7 to AGND; since the sensor gives -voltage under pH 7, I'm using the formula vref/pga/2^23-1 for the positive +7 pH with encouraging results, but using the same formula as (with also -vref/pga/2^23-1) I have wrong numbers. I'm using a Stellaris Cortex M4 as controller.
Our sensor has a an increment of 57 mV/1 pH for the record I can say that I having for example:
with pH ~4.6 16026313 counts,
~6.6 16704756 counts
and ~8 220,00 counts,
Which in some way sense ADS1248 uses signed two's complement any help to convert the counts or any other suggestion will be very appreciated.
Cheers
German