Hi,
we have created a board with ADS1675 relying on original ADS1675 REF project files available on this community.
We wanted to ask help on the operation of the board with reading data generated by ADS1675 through SPI interface. The pins of the chip are configured as follows:
pin30:LVDS 1
pin29:SCLK_SEL 1
pin28:PDWN 1
pin32:LL_CONFIG 0
pin33:FPATH 0
pin34:DRATE2 0
pin35:DRATE1 0
pin36:DRATE0 0
pin38:/CS 0
pin37:START 1 (HOLD HIGH)
pin43:/DOUT floating
pin45:/DRDY floating
letting work the board in single-ended mode (by grounding one of the two inputs) and providing a voltage of 1.5V between an input and ground, a clock signal with f = 10 Mhz on pin 55 and a clock signal SCLK of (pin42) @ 250HZ, pulses HIGH are detected on pin 46 (DRDY), but after this if we try to read the signal on DOUT (pin44) we see DOUT always LOW.
The power supply voltages supplied to the card are +5VAnalog +5VDigital +3.3 VDigital , +9V= VCC and -5V=-VCC for THS4503ID.
You might tell us how to act to test the correct operation of the card? the way in which the pins are configured is correct or should be changed?
All the tests are performed with a single board RIO 9602 card reading and setting ADS1675 pins through DIO connectors.
May i post FPGA code if it is useful to solve the problem or maybe you already have available some labview code to drive ADS1675 with NI sbRIO boards?
Thank you for your attention.
Best Regards.
Eng Mariano Rotunno