We are using 2 ADS1234 ADCs in our circuit. If we use an external clock source to drive both ADCs, will they convert at the same time and remain in sync? If they would remain in sync, we could watch for completion of one conversion (DRDY low) and then clock both conversions out at the same time from both ADCs. Is there any way to get two ADCs in sync? Can I power up an external oscillator first then power up both ADCs later?
Can I power them up (using an external oscillator) and then force them into conversion by clocking out 25 bits? Or can I put both ADCs in STANDBY mode and wake them up together with the SCLK? Would this synchronize them and would they stay in sync?