Other Parts Discussed in Thread: ADS1282
Hi all,
I'm using the ADS1282 in my prototype board. The MFLAG (Modulator Over-Range Detection) signal always outputs high.
Power supply: DVDD=+3.3V, AVDD=+2.5V, AVSS=-2.5V. Voltage reference: VREFP=+2.5V, VREFN=-2.5V. Anolog inputs AIN1P and AIN1N are short-connected for test.
According to the configuration guide in the datasheet, a nRESET signal is needed after power-on. But immediately the MFLAG turns high, which puzzels me a lot. After that the registers can be read or write normally, but when reading the conversion results (either by Read Data Continuous or Read Data By Command Mode), the output data is always 0x7FFFFF.
Best regards
Su Tao