Hi,
I have been using the ADS1282EVM (and MMB0 Rev D) evaluation kit for a while, in a single ended (+5V) mode (using the supplied power pack), with good results (and no power supply related problems).
However, I now have to extend the input range to cover greater than 5V (about 7.5V), so I am trying to use a bipolar power supply (+/-5V) with some problems. I am actually using a battery pack, but I don't think the actual power source matters greatly.
Initially, after reading some other posts to work out how to connect the dual supply (on J14) and set the jumper (on J13) on the MMB0, I successfully connected the +5V to the +5VD connection (and +5VA line, using the J13 +5V/+5VA jumper) and the -5V supply to the -5VA connection. I had not connected to +/-10V supplies at this stage, as I wanted to be sure I had properly connected the +5V analog and digital power. All seemed OK at this stage (I also had not plugged the ADS1282EVM daughter board in just yet either). I connected the MMB0 Gnd to the earth on the battery pack. Voltages were correct and no evidence of excess current drain etc, so next step was to plug in the ADS1282EVM board (still without connecting the +/-VA supplies).
This is where the fun starts. Within probably 10-20 seconds of turning on just the +/-5V (and earth), I could smell an brown burning smell. I disconnected the power and hooked up a voltmeter and (somewhat gingerly) reconnected the +/-5V supply. Again I quickly got a burning smell but had the chance to notice the -5V supply was dropping rapidly – it went down to about –2V and I had to pull the power). One last round of testing confirmed the +5V supply seemed to be holding OK, but for some reason, the -5V supply is being "shorted" by something on the ADS1282EVM board.
I'm embarrassed to mention that the last time, I also saw a wisp of smoke from one of the smaller ICs (but couldn't say which one), as well as the burning smell. Something, somewhere ion the ADS1282EVM is decidedly unhappy about how I’m providing the –5V supply.
Both the +5V and-5V supply provided by fixed voltage regulators (7805 and 7905) and should have ample current to supply the ADS1282EVM (and there was no indication of a hot/blown regulator).
Is there something else that needs to be done to use a -5V supply or do you have any suggestions as to why I am cooking some IC on the ADS1282EVM board, when there was no problem with the -5VA supply when just using the MMB0 board on its own? I'd love to try some more troubleshooting, but I don't think I can chance blowing up the ADS1282EVM (if I haven't already fried something).
Best Regards
Paul Atkins