Other Parts Discussed in Thread: TSW3085EVM
Hello ,
exist a mechanical Drawing from the TSW 1400EVM and the TSW3085EVM?. I want mount this parts with the Standoffs on a ALuminia Board.
In the document from the TSW 1400EVM is described " First connect 5 V Power to the Board, then turn on the Switch SW7"
I want to build the TSW1400EVM , TSW3085EVM, a PC with a Display in a Case with a main power supply ( 5V, 6V, 12 V ) Is it possible to connect all together with the Switch SW7 "On" and then turn on all boards with the main power supply?
Thanks for an answer
best regards Martin