This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

12BIT DAC

Guru 13485 points

Other Parts Discussed in Thread: DAC714, DAC7731, DAC8811, DAC7512

Looking for a DAC, 12bit (or higher)SPI interface,single chanel,with output voltage range of +/-10V.

I found the DAC714/DAC7731,but these are old and  in large package .

Any other recomendation?

  • Eli,

    Is it a requirement that the DAC "natively" outputs the +/-10V signal? There's certainly some methods to generate external circuitry to condition the DAC output to the correct range. This is a pretty common method to achieve the desired output which will open up your range of possible devices.

    What package is most ideal for you? DAC8811 has a smaller package and the EVM can be pretty easily modified to create a +/-10V signal. 

  • Hi,

    Today customer using our DAC7512 (+ OP-AMP from LTC, p/n  LT1112, but they face high output offset.

    This is the reason they think to use other DAC  that has the capability of  +/-10V.

    Other solution is to use different amp.

  • Eli,

    If the DAC itself needs to be able to swing +/-10V without external conditioning then our choices are limited. The DAC7731 would seem to be a pretty nice fit here to me, especially given the benefits of the calibration features it brings to the table...

    I'll stew on this for a bit and see if I can come up with something smaller