This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC121C021 Read Problem

Just tried using this ADC in a design, but the MCU (LPC1765) I2C does not seem to work with this chip.  I ran a logic trace, and while the ADC responds with a ACK to the SLA Write address, it responds with a NAK to the same SLA+R byte.   No question about it, either the edges of the MCU SCL/SDA pulses are not right for this chip, or something is wrong with the I2C interface of the chip.  The waveforms look textbook.  I am trying to read 2 bytes (16b) from any of the 16b regs.  None of them read back, as the ADC fails to ACK the initial send of the SLA+R byte.  Yet it responds (ACKs) with writes to the same SLA address.  I give up,  changing to a different ADC.

  • Trying to get meaningful data our of this, but it acts crazy.  I have a logic analyzer on this as well.

    I get 0xFFFF out of the conv reg, but the doc says the top 4 bits are suppose to be always 0.

    How is that possible?

    Then I set the ALERT reg to 0x03 to clear the Alert flags, and then I get 0xF030 reading the conv reg.

    Also, when I set the Lo/HI limit regs to 0x0000 or 0x0FFF and then read them back,

    I get wacky LO values like 0x000F .  I didn't set that value.

    I keep getting crazy readings from this ADC.  

    What is the magic way to get this thing to just produce real conv data?