I am looking to use the DC offset correction function of the ADS4149 converter.
I note that the converter has a 'FREEZE OFFSET CORRECTION' control which I would assume I apply after the time defined by the 'TIME CONSTANT' has been reached, however I am unclear on what to expect if I don't apply the freeze control.
I am thinking DC offset may be a function of temperature and that if I leave the correcection 'unfrozen' will it continue to remove any offset or will I have to reapply the function again ?