Hello,
I plan to use ADS8363 EVM board as the basis to build an sequential sampling system. This system will be able to work with mux and acquire around 64 channels, and the data rate from the ADS8363 through SPI interface is over 2 Mbps.
Please recommend an MCU EVM with small size and low power consumption (for this system will be a portable system), and have a tool-chain that not too difficult for a beginner.The MCU should have at least 2 SPI interface, because I need another SPI interface to communicate with wireless module.
I search for TI, AM1802 or OMAP-L138 might be a good choice. Please give me some information about them.
Thanks