This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ads1178/74 SPI SCLK ADC CLK relation question

Other Parts Discussed in Thread: ADS1178

Hello Everyone,

I'm writing in regards to the note in the ads1178 datasheet which says, "For best performance, use fSCLK/fCLK ratios of 1, 1/2, 1/4, 1/8, etc." 

I've read other forum questions here in regards to this relationship, but I haven't managed to find one which addresses my concern. My concern is, does this recommendation also suggest a phase alignment between the the two CLK sources to minimize noise in the measurements?  In my current design, I operate both clocks at the same frequency, but due to the way that I operate the SPI with DMA on my microcontroller, the time that I activate the SPI CLK (after respecting the tDS specification) can vary slightly, introducing a small phase shift between the two CLK sources between one data read and another (I've never measured more than a quarter of a cycle phase shift between best and worst).  Given this, should I expect that this behavior may be introducing added noise to my measurements?

Thanks kindly for any time or insights that anyone could provide.

~Gregg

 


  • Hi Gregg,

    The reason that we recommend to have the SCLK and master clock in phase with one another is to keep the noise at a minimum. We found that when they are out of phase, you will see slightly more noise. The noise will still be within spec, but it will be slightly higher with out of phase clocks.

    Regards,

    Tony Calabria