Other Parts Discussed in Thread: ADS131E04
I try to configure ADS131E04. My settings should be:
REG_CONF1 = 0xD1;
REG_CONF2 = 0xE2;
REG_CONF3 = 0xCC;
I have written a function ADS_writereg(uint8_t *buffer,uint8_t startRegAddress, uint8_t regCount) where 2 bytes long WREG opcode is generated like this:
uint8_t bufferTMP[2] = {(startRegAddress | 0x40), regCount-1};
I have defined names for registers like ADS_REG_CONFIG1 is 0x01etc.
When I write my config and read it back I get strange result:
opcode: 11
ADS: d1 e2 cc write: 41 02 d1 e2 cc
OK
read: 20 08 d0 e2 cc 41 00 10 10 10 10
Read data is:
20 08 - opcode RREG startRegAddress 0x00 (ID), regCount=9
D0 - proper ID of ADS131E04 (read-only)
E2 - wrong CONFIG1 data, should be D1
CC - wrong CONFIG2 data, should be E2 like above
41 - wrong CONFIG3 data, should be CC like above
00 - default fault reg value
10 10 10 10 - default settings for channels 1-4
I have noticed recently, that WREG example from datasheet (fig.41) describes writing opcode (OPCODE 1 = 0100 0000, OPCODE 2 = 0000 0001) starting from 0x00 address which is ID register and it's read-only?!
Does it mean that when I pass startRegAddress taken from Table10 to my function I should actually use startRegAddress-1? I can't see that information in datasheet except fig.41 example where read-only ID register is written and I assume someone wanted to write data to CONFIG1 and CONFIG2?
In RREG direct using of startRegAddress seems to work good.
Is it possible to cause any damage by writing improper data to registers? Some of them are described as "Must be set to '1'" and with tries like above this condition wasn't met.