Hello, using the TX-SDK-V1.
Could I connect a transducer and generate a short pulse with the pulser, and then read the signal using the receiver througth the FPGA ?
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello, using the TX-SDK-V1.
Could I connect a transducer and generate a short pulse with the pulser, and then read the signal using the receiver througth the FPGA ?
Thanks.
Hi James,
Using the TX-SDK-V1 you can generate a transmit pulse on a piezotransducer. Then you need to use the analog-front-end like AFE5808 which amplifies, conditions the signal and converts it to digital form, and then you can read and process the data in the FPGA.
Regards, Mariusz