This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS8363 digital input signals with Gatekeeper?

Other Parts Discussed in Thread: ADS8363

Hello,

i have the RD and CONVST signals of the ADS8363 connected together and them connected to a FPGA.

The problem is now, during init/configuration phase of the FPGA after power up, this signal is first a

digital input signal on FPGA side. So i have two inputs connected together.

Worse is, the FPGA input pin has no pull up/pull down resistor active at this moment.

My question is now, does the ADS8363 have a buskeeper/gatekeeper on its input pins?

This would prevent the FPGA input pin from inadvertently clocking during init.

The FPGA input pin is in this init stage a JTAG TCK input pin ;-)
the ADS8363 -CS is always low in my design.