Other Parts Discussed in Thread: ADS1255, ADS1259, THS4521, ADS1278
I have an application using the ADS1255 where it is not practical to use the input buffer due to the constraint on the input range imposed by the buffer. As a result, I need to correct for the finite input impedance of the converter. In order to evaluate the accuracy of this correction, I need to know how reproducible the input impedance is (I know my source impedance very accurately). If possible, I would like to know:
- Unit-to-unit variation
- Drift over time
- Drift over temperature
I am most interested in this information for ADC gains 1 and 4. It would also be helpful to know for gain 32, but that is less important to me because I can use the input buffer in that case.
Thanks for your help.