Other Parts Discussed in Thread: TS3A24159
I'm using TS3A24159 in the following configuration:
Where:
- R13 is open
- PD4 and PB7 are control inputs (Hi or Low)
- VDD: power supply
- I want VXX = VDD only when PD4 is HI
- I want VIN = VBAT only when PB7 is Hi
Is it correct to use:
- COM1 and COM2 as switch ipunts?
- NO1 and NO2 as switch output?
- leaving NC1 and NC2 open (better resistor connecte to GND)?
In my configuration I measure 0.8V on NO1 and N02 when IN1=0 and IN2=0
best regards.