Does anyone have suggestions for an ADC solution with 2 channel, 10 or 12 bit SAR ADC with SPI data output. The one caveat for this part is that we would like the data to clock out on the rising edge of the SPI clock due to some other devices on the SPI bus (we don’t want to have to switch the clock polarity on the fly). It looks like all the options clock data on the falling edge of the SPI clock.
Anyone have suggestions?