The twH and twL timing requirements are a bit ambiguous: Do they mean that and clock pulse, low or high, only has to be at least 20ns, or do they mean me must maintain the duty cycle to be with 40% and 60%, regardless of frequency?
Or, put another way, if I run SCLK at 1MHz during the conversion, can I still have a clock high pulse as small as 20nS, or does it have to be at least 400 ns?
Cheers!