Other Parts Discussed in Thread: OPA2170, ADS1018, MPC506
Hi,
I'm developing a 32 channel PLC analog interface with signal ranges from 0-10V or 4-20mA that will be converted to 0-5V trough a 250ohms sense resistor.
I'm planning to use a resistor voltage divider (factor 1/2) for each channel, a 16:1 mux, an buffer and a ADC.
For the ADC I choose ADS1018, and OPA2170, operating at 5V.
I would like to ask, if someone, for any reason, would advise me to not use HCT4067 and to use MPC506, and why? There is a factor of 10 in price costs.
MPC506 is protected to input over-voltage until 70Vpp by it's internal 1kOhms resistance. HCT4067 has any over-voltage protection, but I could put a resistor in series. I'm also planning to introduce TVS in each input. Will this solve anything?
I've not much experience with industrial environment, so I would like to get more information if this over-voltage protection is a requirement.
Best regards,
A. Paiva