This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Are these parts able to synch at 2.4GHz

Other Parts Discussed in Thread: ADC07D1520, ADC08D1520, ADC08B3000, ADC083000

Anyways, I’ve been trying to get an answer as to whether a few high speed ADC/DAC’s would be synchronizable at 2.4GHz. My customer is doing a point to point backhaul system with 2 ADC’s and 2 DACs per board. Both need to be synchronized at 2.4GHz.  I’ve narrowed it down to these 4 ADC’s because they don’t care about resolution, only sampling rate and ability to synch.  Can you please point me in the right direction?  Also, is there anything high speed (maybe a dual capable of 2.25GHz minimum/channel) on the roadmap? 

ADC07D1520
ADC08D1520
ADC08B3000
ADC083000

And for the DAC I only saw the DAC5670. Is that correct?

THanks in advance.