Hi, I have a question about ADA1015.
Reading datasheet and E2E, I found that this device have virtual reference.
Please let me confirm if my following recognitions are correct.
1) FSR(Virtual Reference) is set by PGA setting, VDD does not affect FSR.
2) The output code would be the same value even if the VDD changes, If the input signal is the same.
--> For example, design with VDD=3.3V or 5.0V would have same output code if the input votage is the save value.
Best Regards,
Kawai