This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Difference between performance of AFE and ADC

Other Parts Discussed in Thread: ADS1255, LMP90100, ADS1232, ADS1230, ADS1231

HI,

A customer is working on IN-Motion weighing scale.

which AFE(LMP90100) is better than ADC(ADS1255) or viceversa.

  • Kaushik,

    That question is like asking which automobile is better.  Both devices are 24 bit, and can do the job.  The ADS1255 is a little lower noise and can run faster.  You really need to do a side by side comparison of the specs relative to price to see which is better.  Also consider the ADS1230, ADS1231 or ADS1232 for weigh scales.

    Best regards,

    Bob B