This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AFE4490 with LED strings

Other Parts Discussed in Thread: AFE4490

Hello. I would like to use AFE4490 in reflective application. For reflective operation to be effective, more than one LED should be used. I could use Tx in Common Anode LED Configuration with external LED supply. There are four LEDs per channel. Here's idea for schematics: 

http://pavlin.si/foto/v/tech/afe4490.JPG.html

Is this OK? Are there any suggestions? "VLED" supplying LED strings would be 4xVfLED+1,4V. What about LED fault detection ?

  • Hello,

    Can you explain more about your application and why do you think you need 4 LEDs?

    Whenever putting 4 LED’s in series, the LED Vf will need to be considered. 

    For common anode configuration, voltage at TXP and TXN pins must not exceed TX_CTRL_SUP voltage i.e., (External supply to LED strings - (4* VfLED) - Vcable ) <= TX_CTRL_SUP

    Another option would be to use higher power led to get the desired light intensity. 

    As for the diagnostics: LED S/C, TXP S/C to Gnd and TXN S/C to Gnd should still work. LED Open should still work provided the LED chain satisfies.

  • Hi  Praveen,

    thank you for your answer. I would like to assemble reflective photometric sensor with photodiode in the center surrounded with LED ring.

    Are there any references on using AFE4490 in reflective applications? 

    Marko

  • Hello Marko,

    There are reference designs on using AFE4490 for reflective applications.
    Unfortunately they are customer specific designs and we will not be able to share that information.