Hello
I would like to store the settings for the CDCE62005 chip in the EEPROM as I need to move away from using the GUI to interfacing to the DAC via the SPI. Unlike the DAC, the CDC chip's SPI pins are not immediately accessible, and thus I would be happy to program it once via the GUI and leave it. The GUI seems to give access to locking the EEPROM permanently, but not just do a "Copy RAM to EEPROM – unlock"
Is this functionality available either via the GUI, or can you provide details on the underlying FTDI driver so that we could develop a quick console application?
Thanks
Andrew