1) If AMC7823's AVDD and DVDD is supplied by 5.5V, can it increase DAC's souring current when output range of DAC is configured to 0~5V?
2) What are capacitive load stability at infinite load and 3kohm load?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Feng,
The AMC7823 is going to have issues driving a 1uF or greater load without adding some series resistance to isolate the output buffer from the load. Unfortunately I don't have a lot of information available to give you about the output amplifier at this time. I am going to work toward developing a model for the DAC outputs for TINA-TI but it may be a while until the complete model is available.
Attached is the only bit of information I've been able to dig up to this point.