Hi,
I am going to buy DAC34H84EVM and fmc-dac-adapter to use it with an FPGA and I have a question concerning the set-up. Before it can be used, I will have to load the firmware via USB from a PC, right?
Will the firmware and configuration stay on the EVM (by EEPROM or something like that) or will I have to load it via USB each time I turn the device off/disconnect power?
If i keep power on 24/7 after the configuration by PC, will I have to reload the firmware at any point of time or will the device run reliably then (for at least a couple of weeks)? Must the PC stay connected? Is there a possibility to run the configuration from the FPGA directly?
Thanks and kind regards
Tobias Rueckelt