Dear sir,
I have to choose LM96551 as my ultrasound HV pulser, but power supply for LM96551 VNN, VPP and VSUB, I can't find any document or reference designs.
Who can help me to make recommendations? Thanks so much.
kuda
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi kuda,
The LM96551 ultrasound HV pulser supply sequence should be started with the VSUB being the most negative potential.
The recommended sequence of power-up & power voltages is (This sequence is required to prevent the part getting blowed up):
The power voltages are based on the Absolute Max. Ratings in the datasheet.
1. VSUB = -65V (it can be as high as -55V with the condition being VPP not being more than +50V)
2. VNN = -50V
3. VLL = 3V
5. VDN & VDD (you can choose to power up VDN before VDD) = -10V & +10V (respectively)
6. Last VPP = +50V
Similarly the power down sequence should be the reverse order:
1. VPP
2. VDD & VDN
3. VLL
4. VNN
5. Last VSUB
The collateral for the reference designs will be made available when you buy the boards at http://www.ti.com/tool/tx-sdk-v1.
Thanks,
Rohit